DIO#.SOURCE
Description
DIO#.SOURCE sets the digital output source when the digital IO pin is configured as an output through DIO#.DIR.
| Value | Description |
|---|---|
| 0 - User | User controls the output value using DIO#.STATEU |
| 1 - Action Table | Action table controls the output value |
| 2 - Fieldbus |
Fieldbus controls the output value |
| 4 - Compare | Compare channel controls the output value |
Examples
Usage
0: User controlled. DIO#.STATE is set by DIO#.STATEU.
1: Action table controlled. DIO#.STATE is set by the assigned action, if any.
2: Fieldbus controlled. DIO#.STATE is set by the fieldbus output control 3681h Digital output control sub 1.
4: Compare channel controlled. DIO#.STATE is set by the compare channel output. The specific channel is selected by DIO#.SOURCEID.
Code
Changing output state with STATEU and then changing SOURCE to be action table with no action configured:
--> DIO1.DIR 1
--> DIO1.SOURCE 0
--> DIO1.STATE 0
--> DIO1.STATEU 1
--> DIO1.STATE 1
--> DIO2.DIR 1
--> DIO2.SOURCE 1
--> DIO2.STATE 0
Context
For more information see Digital Inputs and Outputs.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 | |
| Added Compare source | 02-06-00-000 |
General Information
| Type | Read/Write |
| Units | N/A |
| Range | 0, 1, 2, 4 |
| Default Value | 0 |
| Data Type | Integer |
| See Also | |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
| Fieldbus | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
DIO1.SOURCE | 0x368A | 0x5 | USINT | - | - | RW | False |
| DIO2.SOURCE | 0x368B | 0x5 | USINT | - | - | RW | False | |
| DIO3.SOURCE | 0x368C | 0x5 | USINT | - | - | RW | False | |
| DIO4.SOURCE | 0x368D | 0x5 | USINT | - | - | RW | False | |
| DIO5.SOURCE | 0x368E | 0x5 | USINT | - | - | RW | False | |
| DIO6.SOURCE | 0x368F | 0x5 | USINT | - | - | RW | False |